I make a mistake in rx today . i use the HEW to download the program to the board ,and set write on-chip flash .but when reconnect , it said to put in the id code Verification which
i don't know. hew could i solve this problem,please help ? my device is E1 and RX62N , thank you.
To Erase the part using FDT, do the following:
1. Download FDT and install it.http://am.renesas.com/products/tools/flash_prom_programming/fdt/download_search_results.jsp
2. Open FDT, create a project with settings as in example FDT project "RDK_FDT.zip".
For the YRDKRX62N board:
3. Disable J-Link with jumper.
4. Set Sw3 to SCI Boot setting.
5. Power board using either USB connection.
6. Select "Connect" in FDT.
7. Erase.
Each time you do Disconnect, you must power down device (board) 10 seconds before doing Connect again.