I2C Communication

Can I get the sample code for for RX130 I2C Communication?

I have to send data another controller through I2C.

I am Using RX-130 as a slave.

  • Hello Mr JB sir...

    I get your codes, but this code is not working for RX 130 controller.

    I made all changes as per manual but I am not able to perform I2C application.

    Can I get RX 130 sample code.

  • Hi AJ,

    Apologies for the delayed response. How are things going? Unfortunately, I don't have any sample code anymore as I don't use this device. That sample code should work as it includes the RX130 as a target device. But you should also refer to your device hardware user's manual to see other notes in using the I2C peripheral.

    JB
    If this response, or one provided by another user, answers your question, please verify the answer. Thank you!
    Renesas Engineering Community Moderator
    https://community.renesas.com/
    https://academy.renesas.com/
    https://en-support.renesas.com/knowledgeBase/

  • Hello JB....

    I am trying to solve I2C communication issue from last few days but I am not able to solve this issue yet .I communicate with Renesas forum but I don't get any correct solution. 

    1.Please check my attached  Rx130 sample code with EEPROM.

    2.Please check my  attached screenshot of configuration.

    3.In Interrupt configuration files  I am not able to see the Used interrupt vector.

    I hope above information will help me for solve this issue & I get the correct solution.

    Regards

    AJ

    RX130 with EEPROM.txt
    /*******************************************************************************
    * DISCLAIMER
    * This software is supplied by Renesas Electronics Corporation and is only
    * intended for use with Renesas products. No other uses are authorized. This
    * software is owned by Renesas Electronics Corporation and is protected under
    * all applicable laws, including copyright laws.
    * THIS SOFTWARE IS PROVIDED "AS IS" AND RENESAS MAKES NO WARRANTIES REGARDING
    * THIS SOFTWARE, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING BUT NOT
    * LIMITED TO WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE
    * AND NON-INFRINGEMENT. ALL SUCH WARRANTIES ARE EXPRESSLY DISCLAIMED.
    * TO THE MAXIMUM EXTENT PERMITTED NOT PROHIBITED BY LAW, NEITHER RENESAS
    * ELECTRONICS CORPORATION NOR ANY OF ITS AFFILIATED COMPANIES SHALL BE LIABLE
    * FOR ANY DIRECT, INDIRECT, SPECIAL, INCIDENTAL OR CONSEQUENTIAL DAMAGES FOR
    * ANY REASON RELATED TO THIS SOFTWARE, EVEN IF RENESAS OR ITS AFFILIATES HAVE
    * BEEN ADVISED OF THE POSSIBILITY OF SUCH DAMAGES.
    * Renesas reserves the right, without notice, to make changes to this software
    * and to discontinue the availability of this software. By using this software,
    * you agree to the additional terms and conditions found by accessing the
    * following link:
    * http://www.renesas.com/disclaimer
    * Copyright (C) 2017 Renesas Electronics Corporation. All rights reserved.
    *******************************************************************************/
    
    /*******************************************************************************
    * File Name    : main.c
    * Device(s)    : RX231
    * Tool-Chain   : Renesas RX
    * Description  : This is a simple demo of the RX231 RIIC for the RSKRX231
    *                starter kit (FIT module "r_riic_rx").
    * Operation    : 1. Compile and download the sample code. Click 'Reset Go'
    *                   to start the software.
    * Limitations  :
    *******************************************************************************/
    /*******************************************************************************
    * History : DD.MM.YYYY Version  Description
    *           31.08.2017 1.00     First Release.
    *******************************************************************************/
    
    /*****************************************************************************
    Includes   <System Includes> , "Project Includes"
    ******************************************************************************/
    #include <stdio.h>
    #include <string.h>
    #include "platform.h"
    #include "r_riic_rx_if.h"
    #include "r_riic_rx_config.h"
    #include "r_riic_rx_pin_config.h"
    /*****************************************************************************
     * Global definition
     ******************************************************************************/
    static uint32_t send_count = 0;
    static void master_call_back(void);
    static riic_info_t iic_info_m;
    
    /*******************************************************************************
    * Function Name: main
    * Description  : api demo of riic communication (master send)
    * Arguments    :
    * Return Value :
    *******************************************************************************/
    void main(void)
    {
        uint32_t version_id = 0;
        volatile riic_return_t ret;
        uint8_t addr_eeprom[1] = {0x50};
        uint8_t access_addr1[1] = {0x00};
        uint8_t mst_send_data[8] = {'R','e','n','e','s','a','s','\0'};
    
        iic_info_m.dev_sts = RIIC_NO_INIT;    /*init the riic communication structure*/
        iic_info_m.ch_no = 0;
        iic_info_m.callbackfunc = &master_call_back;
        iic_info_m.cnt2nd = 7;
        iic_info_m.cnt1st = 1;
        iic_info_m.p_data2nd = mst_send_data;
        iic_info_m.p_data1st = access_addr1;
        iic_info_m.p_slv_adr = addr_eeprom;
        printf("iic_info_m.p_data2nd = %s\n",mst_send_data);
    
        ret = R_RIIC_Open(&iic_info_m); /* Open RIIC */
        if (RIIC_SUCCESS != ret)
        {
            printf("Open I2C failed \n");
            return;
        }
        else
        {
            printf("Open I2C success!!\n");
        }
        version_id = R_RIIC_GetVersion();         /* Get RIIC Version ID */
        printf("VersionId = version_id(V%d.%d)\n",((version_id >> 16) & 0x00FF), (version_id & 0x00FF));
    
        ret = R_RIIC_MasterSend(&iic_info_m);    /* RIIC Master Send Start */
        if (RIIC_SUCCESS != ret)                 /* To determine whether the Master send return value is success */
        {
            printf("Master Send failed ,return Value is %d\n",ret);
            R_RIIC_Close(&iic_info_m);
            return;
        }
        else
        {
            while (1)
            {
                if (RIIC_FINISH != iic_info_m.dev_sts)    /* To determine whether the transmission is over */
                {
                    if(RIIC_NACK != iic_info_m.dev_sts)      /* To determine whether the status is NACK */
                    {
                        if(RIIC_TMO != iic_info_m.dev_sts)/* To determine whether the status is TimeOut */
                        {
                            continue;                      /* RIIC Transfer is not Time out,continue wait */
                        }
                        else
                        {
                            printf("RIIC Transfer is Time out\n");     /* RIIC Transfer is Time out */
                            break;
                        }
                    }
                    else
                    {
                        if (send_count >= 200)             /* To determine whether the send count is more than 200s */
                        {
                            printf("the number of send times is %d\n",send_count);
                            break;
                        }
                        else
                        {
                            R_BSP_SoftwareDelay(100, BSP_DELAY_MICROSECS);
                            send_count++;                    /* send count plus 1,and send data once more   */
    
                            iic_info_m.dev_sts = RIIC_NO_INIT;    /*init the riic communication structure*/
                            iic_info_m.cnt2nd = 7;
                            iic_info_m.cnt1st = 1;
                            iic_info_m.p_data2nd = mst_send_data;
                            iic_info_m.p_data1st = access_addr1;
    
                            ret = R_RIIC_MasterSend(&iic_info_m);
                            if (RIIC_SUCCESS != ret)
                            {
                                printf("Master Send failed ,return Value is %d\n",ret);
                                break;
                            }
                            else
                            {
                                printf("the number of send times is %d\n",send_count);
                                continue;
                            }
                        }
                    }
                }
                else
                {
                    printf("iic_info_m.dev_sts = %d\n",iic_info_m.dev_sts);
                    printf("Master send Data has finished\n");
                    break;
                }
            }
        }
        R_RIIC_Close(&iic_info_m);/* RIIC transfer is over ,close the RIIC bus */
        printf("RIIC transfer is over,close the RIIC Channel\n");
        return;
    }
    /*******************************************************************************
    End of function main
    *******************************************************************************/
    
    /*******************************************************************************
    * Function Name: master_call_back
    * Description  : callback function of RIIC API
    * Arguments    :
    * Return Value :
    *******************************************************************************/
    static void master_call_back(void)
    {
        volatile riic_return_t ret;
        riic_mcu_status_t iic_status;
    
        /* Get I2C Status */
        ret = R_RIIC_GetStatus(&iic_info_m, &iic_status);
        if (RIIC_SUCCESS != ret)
        {
            printf("Get I2C Status failed\n");
        }
        else
        {
            printf("iic_status.LONG = %x\n",iic_status.LONG);
        }
    
        return;
    }
    /*******************************************************************************
    End of function master_call_back
    *******************************************************************************/
    
    


  • Hi AJ,

    Unfortunately, I don't have an RX130 on hand so I can't try this one. Have you tried debugging it? What errors are you receiving? Did you successfully open the I2C port when you call the R_RIIC_Open() function? What return value did it return?

    JB
    If this response, or one provided by another user, answers your question, please verify the answer. Thank you!
    Renesas Engineering Community Moderator
    https://community.renesas.com/
    https://academy.renesas.com/
    https://en-support.renesas.com/knowledgeBase/