Open drain pin configuration for GPIO P22/P23 Rx130 part number R5F51306B

We are using RX130 controller part number R5F51306B for one of our projects. We have developed our customized development board in which there is no external circuit connected to controller pins.

So, any external devices/interface such as EEPROM, RTC etc., that are going to be connected to controller; those are having their own small PCBs and circuits on them, and we then connect their input/output directly controller pins.

 I am facing an issue with open drain configuration for couple of IOs as listed below –

Our understanding of Open Drain –

  1. Unless external pull up is connected to these pins pin shall not be driven high

 Is this understanding, correct?

 Issue I am facing –

 Even though I have not connected any external pull-up to above pins I see pin can be toggled between HIGH and LOW.

Still issue persists!!

Also, I see ODR0 register have correct configuration (B6 & B4 bit in ODR0 must be set to 1 for open drain as per datasheet).

Still open drain configuration functionality is not as expected.

Parents Reply Children
No Data