Dear team,
My customer wants a permanent license for the professional version of our Compiler for RX but has two questions.
1. What property of the computer is used for the node-locked version?
2. What version of Windows is required for each of the two versions (node-locked / floating)?
Waiting for your kind feedback, thanks a lot.
Regards,
Shai
Hello Shai,
Please refer to this page to find the hardware and software requirements
https://www.renesas.com/us/en/software-tool/system-requirements
They are not dependent only on the compiler itself but on the IDE you are using as well.
Kind regards,
Sergey
If this response, or one provided by another user, answers your question, please verify the answer. Thank you!
Renesas Engineering Community Moderatorhttps://community.renesas.com/https://academy.renesas.com/https://en-support.renesas.com/knowledgeBase/
Hi Sergey,
1. The customer needs only one station, so what is the difference between the professional version and the standard version?
As for a yearly vs. permanent license, If they purchase a permanent license, then the decision between node-based and floating would, again, be based on the pricing, as well as on the conditions of the node-based option.
2. It raises another question for instance, if the node-based option is dependent on the serial number of a hard drive, then this means that the license isn't really permanent - it will last only for the life of the disk which is about 5 years OR the permanent node-locked license could be transported into different PC in case the PC got broken/replaced?
Waiting for your kind feedback on the subject, thanks in advance.
Hi Shai Berman.These links should answer your question:https://tool-support.renesas.com/autoupdate/support/onlinehelp/csp/V8.05.00/CS+.chm/Compiler-CCRL.chm/Output/ccrl01c0500y.htmlhttps://en-support.renesas.com/knowledgeBase/18516988Regards,Jayesh If this response, or one provided by another user, answers your question, please verify the answer. Thank you!Renesas Engineering Community Moderatorshttps://community.renesas.com/https://academy.renesas.com/en-support.renesas.com/.../
Jayesh (SWF) Hello,
Thanks a lot, could you please indicate what information is used to identify the node so that they can assess the lifetime of the license?
Hi Shai Berman.Let me get details about this from the internal team and then I'll get back to you.Regards,Jayesh