USB Data Acquisition, CY7C68013A with RX23E-B

Hi,

RX23E-B with analogue front end is a cool chip, I'm thinking to make a DAQ based on it. Infineon/Cypress's CY7C68013A USB chip is used in some DAQs, CY7C68013A uses a parallel interface to get data from ADC chips for a fast transfer speed, does RX23E-B supports parallel interface between USB chip like 68013?

Why I mention 68013 is it has software supports in Windows and Linux.

ADC at 125kSPS, the data rate is 125k*3 bytes = 375k bytes/second, my worry is UART may not be fast enough.

Thank you.