Can I use the USB function even if I use HOCO as the PLL source?

In the manual, it is stated as follows. It is interpreted that the USB is affected.

However, on our board, USB works well even with HOCO.

I'm curious if it's really usable, or if it only affects certain USB functions.

Please help me with this issue.

Parents Reply Children
No Data