Hi,
I am trying to read and write eeprom M24256.
I have used smart configuration but I am not able to read data in random address read.
Datasheet related eeprom said:
Random Address Read:
A dummy write is performed to load the address into the address counter. Then, without sending STOP condition, the master sends another START condition, and repeats the Device Select Code, with the RW bit set to 1. The memory acknowledges this, and outputs hte contents of the adressed byte. The master must not acknowledge the byte output, and terminates the transfer with stop condition.
Could you indicate to me how can manage this situation ?
Br,