rx-231 SCI6 as SPI

Dear All

I want to use RX-231 SCI6 (pin 16, 17, 18) to read / write data to external RAM.

Is there any sample code about this ?

regard,

rachmat

Parents Reply
  • What is the reason of use FIT module (and smart config)? SPI setup on 231 is really simple:

    1. setup port1 (chapter 22 of RX231 HW manual)

    2. setup SCI6 fo SPI (chapter 33 of RX231 HW manual)

    3. write service routine for read/write

    Enjoy your system working...

    and throw away all that junk with FIT and smart config...

Children
No Data