Headless build with configurable Linker sections

I am hoping to build two application images (with same application)  with the headfless build option 

Application2 Start Address           0xFFE90000
Application2 Exception Vector      0xFFF27F70
Application2 Reset Vector             0xFFF27FEC

Application1 Start Address           0xFFF28000
Application1 Exception Vector     0xFFFBFF70
Application1 Reset Vector           0xFFFBFFEC

Currently I am able to build  by manually editing the linker options in E2Studio project options but wish to automate the build process using the headless build option.

Is it possible to feed the section address  to headless build option?

Thanks so much

Parents
  • Hello,

    Please check the link below on how to use e2studio with eclipse/CDT feature:

    https://en-support.renesas.com/knowledgeBase/16979374

    You will need something like the command  below:

    e2studioc.exe -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "c:\wksp" -import "c:\wksp\MyProj" -build

    and implement it twice for the two different build configurations from two different projects ( two projects for the two applications)

    About motorola format, something like the below maybe matches with your case:

    objcopy -O srec <input_file>.abs  <output_file>.srec

    Input_file.abs will be the generated file after the build command.

    Another option and more general with more capabilities would be to create a makefile as mentioned from Jimb that will specify  how to compile and link your project using CC-RX toolchain

    Regards,

    AL_Renesas

Reply
  • Hello,

    Please check the link below on how to use e2studio with eclipse/CDT feature:

    https://en-support.renesas.com/knowledgeBase/16979374

    You will need something like the command  below:

    e2studioc.exe -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "c:\wksp" -import "c:\wksp\MyProj" -build

    and implement it twice for the two different build configurations from two different projects ( two projects for the two applications)

    About motorola format, something like the below maybe matches with your case:

    objcopy -O srec <input_file>.abs  <output_file>.srec

    Input_file.abs will be the generated file after the build command.

    Another option and more general with more capabilities would be to create a makefile as mentioned from Jimb that will specify  how to compile and link your project using CC-RX toolchain

    Regards,

    AL_Renesas

Children