Headless build with configurable Linker sections

I am hoping to build two application images (with same application)  with the headfless build option 

Application2 Start Address           0xFFE90000
Application2 Exception Vector      0xFFF27F70
Application2 Reset Vector             0xFFF27FEC

Application1 Start Address           0xFFF28000
Application1 Exception Vector     0xFFFBFF70
Application1 Reset Vector           0xFFFBFFEC

Currently I am able to build  by manually editing the linker options in E2Studio project options but wish to automate the build process using the headless build option.

Is it possible to feed the section address  to headless build option?

Thanks so much

Parents Reply Children
No Data