hi
i am working on the Renesas RX63N MCU,
i am getting the dialouge box of "ID code verification" while connecting through the E1 debugger.. but i have not set any password for flash in my code.
pls provide the solution for this asap and also the cause.
its urgent..
thank u. :)
what do u mean by pin output setting(high) 0x36 ???
pls brief....
When you connect the e1 in generic boot mode using FDT you should be presented with a window to select which pins are used as output and which of these are set high. Do you get this option?
If you do then set the Pin Output row such that the end result give 0x36. This should be io1 to io4. Then we don't set any high so the Pin Setting(High) row should be 0. These could be different depending on your hardware.
Hola buenas,
Compre unas CPUs en china , y no hay manera de poder acceder a ellas
me pide Código de verificación entro FFFFFFFFF- ó 0000000000-
y no hay manera lo hago a través de E8a
me podrían comentar como tengo de proceder oh TIRARLOS
Agradecido