Hi,
can you please guide me how to update code of RX71m MCU using FTD(SCI boot)
is any operation manual/code sample available for that
what type of hardware connection i need to do?
What type of software interface i have to use ?
please suggest
Hello,
You can use as reference the application note below, that implements a SCI bootloader on RX140:
Ιt uses Xmodem protocol to transfer the image from the user's PC folder location to the internal flash of the RX.
https://www.renesas.com/en/document/apn/renesas-starter-kit-rx140-boot-loader-application-note
Also, on the link below, you can find the projectd for the bootloader and for the application on CS+:
https://www.renesas.com/en/document/scd/rx140-renesas-starter-kit-sample-code-cs-cc-rx?r=1618031
Τhe same idea can be implemented on RX71M.
Regards,
AL_Renesas
Hi AL_Renesas San,
Thanks for the replay,
Actually, i was expected the replay Which is given By JimBsan
But The response given by you is more interested can you please check & confirm details..
please confirm i will explain what i understand,
1. First we have to define Boot loader Program with condition of checking input from user for updating firmware or not .
2. load the boot loader program on the MCU using Debugger (E2 lite,E1 etc).
3. Restart the MCU Generate the condition of erasing application Code & update previous code with new One.
Now the my question is that
Is we need to use any dedicated port for SCI