Compiler warnings settings cleared by build proccess

e2 studio version: 2024-10

GCC: 8.30

In progect properties C/C++ Build-> Settings ->Tool Settings ->Warninings if  compiler warnings -Wall and -Wextra are enabled it works as expected on builds.  If after enabling the warnings Project->Clean is run with start a build immediately. It disables the compiler warnings(-Wall and -Wextra) in the project settings before building.

Is there a way to prevent the compiler warnings from being disabled after a clean and build?

Note: I belive the compiler warnings in project settings are reset to default by the "SC code Generation Builder" as disabling the builder stops this from happening