The datasheet shows the RX72M (like the RX72N) have a onboard Graphic LCD controller. But after creating a project with R5F572MDDxFP in e2studio with smart configurator, under Pin configuration there is no Graphic-LCD Controller hardware resource, like there is with for example a R5F572NDDxFP
Is that because of a bug with E2 studio or is the datasheet for the RX72M wrong?
Did you download the FIT driver module. Add component Search for Graphic then pull down the driver module and add the three parts for the graphic in the components view.
Otherwise you could Submit a Ticket to the technical support system and attach your project for review.
Hello,
If you are using Smart Configurator with RX72M, you can add the r_glcdc_rx module that also configures the pins for the LCD:
The same pins can be found on the Pins tab,if you select Graphic-LCD controller:
Regards,
AL_Renesas
You did not try it with my specific MCU (R5F572MDDxFP) as your screenshots show a BGA chip. Please read my 1st post again. Also, I can add the r_glcdc_rx module just fine. The Graphic-LCD Controller only shows in Pin configuration if the part is a R5F572NDDxFP... but not if the part is a R5F572MDDxFP.
RX72M :-
RX72N :-
Thanks.