The datasheet shows the RX72M (like the RX72N) have a onboard Graphic LCD controller. But after creating a project with R5F572MDDxFP in e2studio with smart configurator, under Pin configuration there is no Graphic-LCD Controller hardware resource, like there is with for example a R5F572NDDxFP
Is that because of a bug with E2 studio or is the datasheet for the RX72M wrong?
Hello,
If you are using Smart Configurator with RX72M, you can add the r_glcdc_rx module that also configures the pins for the LCD:
The same pins can be found on the Pins tab,if you select Graphic-LCD controller:
Regards,
AL_Renesas
You did not try it with my specific MCU (R5F572MDDxFP) as your screenshots show a BGA chip. Please read my 1st post again. Also, I can add the r_glcdc_rx module just fine. The Graphic-LCD Controller only shows in Pin configuration if the part is a R5F572NDDxFP... but not if the part is a R5F572MDDxFP.
RX72M :-
RX72N :-
Thanks.