How to implement SPI interface in RX631

Hi all,

 I have to update an old project made with HEW (High-performance Embedded Workshop).

The micro is from the RX631 family (R5F5631BDDFB).

I have to implement an SPI peripheral in master mode (SPI7 on pins P90, P91, P92, P93). I have never implemented SPI before.

I would like to keep the project in HEW.

Could you tell me if there are any application notes or portions of code to understand how to implement it?

I would need to know how to configure the registers, the functions for reading-writing etc..

thanks

Stefano

Parents Reply Children
  • Thanks for the help.

    I'll try to do as you suggested.
    It would be nice to have an old version of the smart configurator for RX63

  • The Applilet4 preceded the Smart Configurator tool and I don't see support for RX63 devices with it, unfortunately.  I guess the RX63 was effectively obsoleted by the time these code generating tools became available.

    Unless someone from Renesas has a better suggestion or can dig up some sample code, I believe your best approach would be to try using the code generated from the Smart Config tool as previously mentioned as a starting point.

  • That's right, Rx63 devices are older than applilet.
    If there is no sample code available I will do as you suggested.

  • I happened to stumble upon a RX63N sample project that includes RSPI driver for RX compiler v1.02:

    RX600 Series Hardware Data Collection and Filtering using the RX63N

    Look in the folder "Workspace\rx_hw_datacollection\r_rspi_rx".

    PLEASE REFER TO THE APPLICATION NOTE FOR THIS MIDDLEWARE FOR MORE INFORMATION
    
    RX RSPI Driver
    ==============
    
    Document Number 
    ---------------
    N/A
    
    Version
    -------
    v1.40
    
    Overview
    --------
    Basic RSPI Master Mode driver. 
    
    Features
    --------
    * Functions to init, read, and write the RSPI channels
    * Ability to lock channels to a task to ensure no other tasks try to use peripheral while it is already being used.
     
    Supported MCUs
    --------------
    * RX621, RX62N Group
    * RX630 Group
    * RX631, RX63N Group 
    
    Boards Tested On
    ----------------
    * RSK+RX62N
    * RDKRX62N
    * RSKRX63N
    * RDKRX63N
    
    Limitations
    -----------
    * This code is not re-entrant but does protect against multiple concurrent function calls.
    
    Peripherals Used Directly
    -------------------------
    * RSPI0
    * RSPI1
    * RSPI2
    
    Required Packages
    -----------------
    * none
    
    How to add to your project
    --------------------------
    * Add src\r_rspi_rx.c to your project.
    * Add an include path to the 'r_rspi_rx' directory. 
    * Add an include path to the 'r_rspi_rx\src' directory.
    * Configure middleware through r_rspi_rx_config.h.
    * Add a #include for r_rspi_rx_if.h to files that need to use this package. 
    
    Toolchain(s) Used
    -----------------
    * Renesas RX v1.02
    
    File Structure:
    ---------------
    r_rspi_rx
    |   readme.txt
    |   r_rspi_rx_config.h
    |   r_rspi_rx_if.h
    |
    \---src
            r_rspi_rx.c
                    
    

  • Hi Jim, thanks again for the support! I'll try your suggestions

  • Hi Jim,
    I did it.
    I didn't use "RX600 Series Hardware Data Collection and Filtering using the RX63N" ​​because the project contains a RSPI, while I use a standard SPI (SCI7).
    I used Smart Configurator for RX671 and adapted the code to the old HEW environment.
    Thanks again!