This is an e2 studio sample project using CCRX compler.
It shows a project where the program uses an ID code for flash protection.
The RFP project includes the ID code for verification, but will open a ID verification dialog.
Hello. I can not put the IDCODE and Control code into the flash by connecting with debugger.
Is it only possible to do it with RFP during boot mode? Or can I do it with HEW or E2STUDIO in debugging?
Does it depend on the cpu operating mode?