Dear all,
"macnica-ae@macnicaae-Precision-7520:~/user/rzv2m_bsp/build$ bitbake core-image-minimalERROR: Unable to start bitbake server (None)ERROR: Server log for this session (/home/macnica-ae/user/rzv2m_bsp/build/bitbake-cookerdaemon.log):--- Starting bitbake server pid 10046 at 2023-03-20 12:21:41.819667 ---ERROR: The following required tools (as specified by HOSTTOOLS) appear to be unavailable in PATH, please install them in order to proceed: ar as chrpath diffstat g++ gawk gcc ld make nm objcopy objdump ranlib readelf rpcgen strings strip"
I struct in this issue,please gave solution for above attached image.
thanks and regards
Aravind S
Remove the "\" from the 1st sudo apt-get install command and try again.
same thing happen sir.
kindly find the attached image, same problem occur it.
Well... Then I would try to simply install the missing required tools as per error.
sudo apt install ar as ...
Sure that you use the correct Ubuntu Version?$lsb_release -r -s18.04The following works for me (it is a little bit more than you really need):$apt-get update$apt-get install gawk wget git diffstat unzip texinfo gcc-multilib build-essential chrpath socat cpio$apt-get install python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping $apt-get install libsdl1.2-dev python$apt-get install p7zip-full python3-git python3-jinja2 libegl1-mesa pylint libssl-dev flex bison$apt-get install libasound2-dev$apt-get install libcurl4-openssl-dev libdbus-1-dev libdbus-glib-1-dev libgconf2-dev$apt-get install libgtk2.0-dev libgtk-3-dev$apt-get install libpulse-dev libx11-xcb-dev libxt-dev libncurses5-dev sharutils cmake zip rsync$apt-get install curl srecord wiggle pbzip2 pigz