RZ/A2M Simple Applications Package V8.40 rza2m_fw_update_sample_freertos_gcc question

Hardware

RZ/A2M-Evaluation-Kit

 

Software

RZ/A2M Simple Applications Package V8.40

e2 studio V2022-01

GNU Arm Embedded Toolchain 9-2020-q2-update

 

Issue

Consult linker_script.ld from rza2m_fw_update_sample_freertos_gcc then modify this file in rza2m_blinky_sample_freertos_gcc.

Build rza2m_blinky_sample_freertos_gcc.bin.

Use image-gen.py from rza2m_fw_update_sample_freertos_gcc to generate userprog.rsu.

Programming userprog.rsu by rza2m_fw_update_sample_freertos_gcc through UART.

Power off and on the RZ/A2M-Evaluation-Kit, the program is running well that can see prompt in UART and LED is blinky.

 

Consult linker_script.ld from rza2m_fw_update_sample_freertos_gcc then modify this file in rza2m_usbh_msc_sample_freertos_gcc.

Build rza2m_usbh_msc_sample_freertos_gcc.bin.

Use image-gen.py from rza2m_fw_update_sample_freertos_gcc to generate userprog.rsu.

Programming userprog.rsu by rza2m_fw_update_sample_freertos_gcc through UART.

Power off and on the RZ/A2M-Evaluation-Kit, program is not running well that only see partial prompt in UART and USB isn't work.

After adding debug message in program (rza2m_fw_update_sample_freertos_gcc), found the program is stock at function usbh0_hstd_ehci_init() because USB00.USBSTS.BIT.PeriodicScheduleStatus=0.

But USB00.USBSTS.BIT.PeriodicScheduleStatus=1 in the original version.

 

rza2m_usbh_msc_sample_freertos_gcc/generate/sc_drivers/r_usbh0/basic/src/r_usbh0_hehci_main.c

uint32_t usbh0_hstd_ehci_init(void)

{

...

    addr = usbh0_hstd_ehci_get_periodic_frame_list_addr();

    R_MMU_VAtoPA(addr,&USB00.PERIODICLISTBASE.LONG);

 

    /* Enable Periodic Schedule */

    USB00.USBCMD.BIT.PeriodicScheduleEnable = 1;

 

    timeout = 0;

    while (0 == USB00.USBSTS.BIT.PeriodicScheduleStatus)

    {

        if (timeout > USBH0_EHCI_TIMEOUT)

        {

            USBH0_HCI_PRINTF0_R("Error : usbh0_hstd_EhciInit TIMEOUT\n");

            return USBH0_ERROR;

        }

 

        r_usbh0_hstd_hci_wait_time(1);

        timeout++;

    }

 

Attachments

rza2m_blinky_sample_freertos_gcc/linker_script.ld

rza2m_usbh_msc_sample_freertos_gcc/linker_script.ld

linker_script.zip

Parents
  • Could you change "r_startup_config.h" in "rza2m_fw_update_sample_freertos_gcc" and try?

    Please change USB to USE as follows.
    /* select whether USB0 use or not
    * 0 : Use USB0
    * 1 : Not use USB0
    */
    #define STARTUP_CFG_DISABLE_USB0 (0)

    /* select whether USB1 use or not
    * 0 : Use USB1
    * 1 : Not use USB1
    */ /* select whether USB1 use or not * 0 : Use USB1 * 1 : Not use USB1
    #define STARTUP_CFG_DISABLE_USB1 (0)

Reply
  • Could you change "r_startup_config.h" in "rza2m_fw_update_sample_freertos_gcc" and try?

    Please change USB to USE as follows.
    /* select whether USB0 use or not
    * 0 : Use USB0
    * 1 : Not use USB0
    */
    #define STARTUP_CFG_DISABLE_USB0 (0)

    /* select whether USB1 use or not
    * 0 : Use USB1
    * 1 : Not use USB1
    */ /* select whether USB1 use or not * 0 : Use USB1 * 1 : Not use USB1
    #define STARTUP_CFG_DISABLE_USB1 (0)

Children
No Data