First time posting here!
This is a strange problem that I am trying to isolate. I would appreciate any ideas about the issue.
I am having issues with making a wired connection on newer routers. My device connects properly to my older router and also is able to connect if I create a bridge to the Ethernet port on my Mac-book.
The problem seems to arise on newer routers. I was first unable to connect to my ISP’s router, so I bought a newer router and have the same problem. Here’s some of the details.
First of all the lights on my Ethernet port do not even flicker with the newer routers. If I connect the Ethernet to the Ethernet port on my Mac-book, it instantly flickers and works.
vEtherISRCallback will not be called on these newer devices, but will immediately be triggered when plugged into the older routers.
My device sends out a DHCP discover, but I am thinking the problem is at the Ethernet level due to this interrupt not being triggered? Could there be a newer protocol on these newer devices that I am not aware of?
Any thoughts would be appreciated, even brainstorming.
I think you are correct that it's not a DHCP. Is your PHY on your board setup to auto negotiate the speed between 10/100/1000BaseT and full/half-duplex? Is the router (actually you sound like you're using a Layer 3 switch or similar) set up to handle negotiating a normal or uplink port automatically or are you using a cross-over cable accidentally?
Also, by "my device", is this some sort of Renesas eval board? What kind and what are you running?
-Larry
Thanks Larry for the response!From what I can see I believe that we can do 10/100 for negotiation, but I don't see 1000. I believe Half/Full duplex is supported for both 10/100.For routers that did not work I used my ISP's router. This is a Telus Wifi Hub, no real model name unfortunately. Secondly I used an Eero 6+ router.
It does not look like I am using a cross over cable, and I have tested with multiple different cables. I am using a custom board, but the Rareness controller is the RA6M3 A6M3AF3CFC.Also please let me know if you need any further explanation from me. I am semi new to this, so will let you know if I am ever not following along.
Can you post the configuation of your ethernet and PHY from the graphic setup in the IDE.
Thanks
Lc
Hi Larry,
Are these the photos that you were requesting? See attached images below.
Hello,
Thanks for reaching out Renesas Engineering Community!
Could you please provide us the part number of the MCU are you using and also are you using a custom pcb board or an evaluation kit from Renesas?
Thank you!
Best Regards,
IK
Hello IK, the part number for the MCU is R7FA6M3AF3CFC#AA0. I am using a custom PCB board.