Hello,
I am using EK-RA2L1 board with device R7FA2L1AB2DFP. Trying to follow the steps mentioned in Secure Bootloader for RA2 MCU Series.
I am using Swap upgrade mode with Signature.
I came across the following error while building the project (tried clean + build too).
Building target: ra2l1_mcuboot_swap_bootloader.elf
c:/renesas/ra/e2studio_v2023-10_fsp_v5.0.0/toolchains/gcc_arm/12.2.mpacbti-rel1/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe:fsp.ld:170 cannot move location counter backwards (from 00000536 to 00000400)
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:102: ra2l1_mcuboot_swap_bootloader.elf] Error 1
"make -r -j16 all" terminated with exit code 2. Build might be incomplete.
Can you please help me solve this error ?
Below I am attaching the images for the some major changes I have made acc to the manual.
Thank You.
Kind Regards,
Keniz Gandhi
Hello Keniz,
Any feedback? Have you tested the project I shared with you?
Regards,
IK
Hi IK,
I didn't check that. However, I solved it. I just changed the address in fsp.ld file and it worked.
Thanks for providing us your feedback, Keniz.
Best Regards,