Hello,
I'm currently facing a problem regarding the erase-part of my flash process. An older version of my code (with the same Debug configuration/ Makefile etc...)used to work perfectly fine. After working on my USB peripheral I noticed that neither the current state, nor the older state of my code, flashes properly anymore. When Debuggin/Flashing the Device i get the following output:
SEGGER J-Link GDB Server V7.94j Command Line Version JLinkARM.dll V7.94j (DLL compiled Feb 14 2024 15:36:06) Command line: -if swd -device R7FA6M1AD -endian little -speed auto -port 2331 -swoport 2332 -telnetport 2333 -vd -ir -localhostonly 1 -singlerun -strict -timeout 0 -nogui -----GDB Server start settings----- GDBInit file: none GDB Server Listening port: 2331 SWO raw output listening port: 2332 Terminal I/O port: 2333 Accept remote connection: localhost only Generate logfile: off Verify download: on Init regs on start: on Silent mode: off Single run mode: on Target connection timeout: 0 ms ------J-Link related settings------ J-Link Host interface: USB J-Link script: none J-Link settings file: none ------Target related settings------ Target device: R7FA6M1AD Target device parameters: none Target interface: SWD Target interface speed: auto Target endian: little Connecting to J-Link... J-Link is connected. Firmware: J-Link OB-S124 compiled Dec 13 2023 14:39:54 Hardware: V1.00 S/N: 831729554 Checking target voltage... Target voltage: 3.30 V Listening on TCP/IP port 2331 Connecting to target... Initializing CPU registers...Connected to target Waiting for GDB connection...Connected to 0000:0000:0000:0000:0000:0000:0000:0001 GDB client (conn. 956) requested target.xml from GDB Server Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x00000000 Read register 'r1' (4 bytes) from hardware: 0x00000000 Read register 'r2' (4 bytes) from hardware: 0x00000000 Read register 'r3' (4 bytes) from hardware: 0x00000000 Read register 'r4' (4 bytes) from hardware: 0x00000000 Read register 'r5' (4 bytes) from hardware: 0x00000000 Read register 'r6' (4 bytes) from hardware: 0x00000000 Read register 'r7' (4 bytes) from hardware: 0x00000000 Read register 'r8' (4 bytes) from hardware: 0x00000000 Read register 'r9' (4 bytes) from hardware: 0x00000000 Read register 'r10' (4 bytes) from hardware: 0x00000000 Read register 'r11' (4 bytes) from hardware: 0x00000000 Read register 'r12' (4 bytes) from hardware: 0x00000000 Read register 'sp' (4 bytes) from hardware: 0x00000000 Read register 'lr' (4 bytes) from hardware: 0x00000000 Read register 'pc' (4 bytes) from hardware: 0x00000000 Read register 'xpsr' (4 bytes) from hardware: 0x00000001 Read 4 bytes @ address 0x00000000 (Data = 0x1FFE3580) Read 2 bytes @ address 0x00000000 (Data = 0x3580) Received monitor command: speed 1000 Target interface speed set to 1000 kHz Received monitor command: clrbp Received monitor command: reset Resetting target Received monitor command: halt Halting target CPU... ...Target halted (PC = 0x000005B4) Received monitor command: regs R0 = 1FFE3578, R1 = 0000FFC3, R2 = 00000000, R3 = 4001C11C R4 = 1FFE0904, R5 = 1FFE0924, R6 = 1FFE0924, R7 = 1FFE3578 R8 = 3CD9DB0A, R9 = 97383CD9, R10= 829F9F7C, R11= 2AFEB3C2 R12= 1FFE0888, R13= 1FFE3580, MSP= 1FFE3580, PSP= AA621784 R14(LR) = FFFFFFFF, R15(PC) = 000005B4 XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000 CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00 Security extension regs: MSP_S = 00000000, MSPLIM_S = 00000000 PSP_S = 00000000, PSPLIM_S = 00000000 MSP_NS = 1FFE3580, MSPLIM_NS = 00000000 PSP_NS = AA621784, PSPLIM_NS = 00000000 CONTROL_S 00, FAULTMASK_S 00, BASEPRI_S 00, PRIMASK_S 00 CONTROL_NS 00, FAULTMASK_NS 00, BASEPRI_NS 00, PRIMASK_NS 00 Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x7835FE1F Read register 'r1' (4 bytes) from hardware: 0xC3FF0000 Read register 'r2' (4 bytes) from hardware: 0x00000000 Read register 'r3' (4 bytes) from hardware: 0x1CC10140 Read register 'r4' (4 bytes) from hardware: 0x0409FE1F Read register 'r5' (4 bytes) from hardware: 0x2409FE1F Read register 'r6' (4 bytes) from hardware: 0x2409FE1F Read register 'r7' (4 bytes) from hardware: 0x7835FE1F Read register 'r8' (4 bytes) from hardware: 0x0ADBD93C Read register 'r9' (4 bytes) from hardware: 0xD93C3897 Read register 'r10' (4 bytes) from hardware: 0x7C9F9F82 Read register 'r11' (4 bytes) from hardware: 0xC2B3FE2A Read register 'r12' (4 bytes) from hardware: 0x8808FE1F Read register 'sp' (4 bytes) from hardware: 0x8035FE1F Read register 'lr' (4 bytes) from hardware: 0xFFFFFFFF Read register 'pc' (4 bytes) from hardware: 0xB4050000 Read register 'xpsr' (4 bytes) from hardware: 0x00000001 Received monitor command: speed auto Select auto target interface speed (2000 kHz) Received monitor command: flash breakpoints 1 Flash breakpoints enabled Received monitor command: semihosting enable Semi-hosting enabled (Handle on breakpoint instruction hit) Received monitor command: semihosting IOClient 1 Semihosting I/O set to TELNET Client Received monitor command: SWO DisableTarget 0xFFFFFFFF SWO disabled successfully. Received monitor command: SWO EnableTarget 0 0 0x1 0 SWO enabled successfully. Read 4 bytes @ address 0x000005B4 (Data = 0xAF00B580) Downloading 16112 bytes @ address 0x00000000 - Verified OK Downloading 7672 bytes @ address 0x00003EF0 - Verified OK Downloading 8 bytes @ address 0x00005CE8 - Verified OK Downloading 1128 bytes @ address 0x00005CF0 - Verified OK Writing register 'pc' = 0x0000385C Comparing flash [....................] Done. Erasing flash [....................] Done. ERROR: Failed to erase sectors 0 @ address 0x00000000 ((erase error)) Failed to erase sectors. Read 4 bytes @ address 0x0000385C (Data = 0x37084618) Reading 64 bytes @ address 0x00000800 Read 2 bytes @ address 0x0000081C (Data = 0xF3C2) Reading 64 bytes @ address 0x00003840 Read 2 bytes @ address 0x00003864 (Data = 0xB480) Reading 64 bytes @ address 0x00000580 Read 2 bytes @ address 0x000005B8 (Data = 0xF000) Read 2 bytes @ address 0x000005E4 (Data = 0xFA5F) Read 2 bytes @ address 0x0000081C (Data = 0xF3C2) Read 2 bytes @ address 0x000005E0 (Data = 0xF867) Received monitor command: clrbp Received monitor command: reset Resetting target Received monitor command: halt Halting target CPU... ...Target halted (PC = 0x000005B4) Read 2 bytes @ address 0x000005B8 (Data = 0xF000) Received monitor command: regs R0 = 00000000, R1 = 0000FFC3, R2 = 00000000, R3 = 4001C11C R4 = 1FFE0904, R5 = 1FFE0924, R6 = 1FFE0924, R7 = 1FFE3578 R8 = 3CD9DB0A, R9 = 97383CD9, R10= 829F9F7C, R11= 2AFEB3C2 R12= 1FFE0888, R13= 1FFE3580, MSP= 1FFE3580, PSP= AA621784 R14(LR) = FFFFFFFF, R15(PC) = 000005B4 XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000 CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00 Security extension regs: MSP_S = 00000000, MSPLIM_S = 00000000 PSP_S = 00000000, PSPLIM_S = 00000000 MSP_NS = 1FFE3580, MSPLIM_NS = 00000000 PSP_NS = AA621784, PSPLIM_NS = 00000000 CONTROL_S 00, FAULTMASK_S 00, BASEPRI_S 00, PRIMASK_S 00 CONTROL_NS 00, FAULTMASK_NS 00, BASEPRI_NS 00, PRIMASK_NS 00 Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x00000000 Read register 'r1' (4 bytes) from hardware: 0xC3FF0000 Read register 'r2' (4 bytes) from hardware: 0x00000000 Read register 'r3' (4 bytes) from hardware: 0x1CC10140 Read register 'r4' (4 bytes) from hardware: 0x0409FE1F Read register 'r5' (4 bytes) from hardware: 0x2409FE1F Read register 'r6' (4 bytes) from hardware: 0x2409FE1F Read register 'r7' (4 bytes) from hardware: 0x7835FE1F Read register 'r8' (4 bytes) from hardware: 0x0ADBD93C Read register 'r9' (4 bytes) from hardware: 0xD93C3897 Read register 'r10' (4 bytes) from hardware: 0x7C9F9F82 Read register 'r11' (4 bytes) from hardware: 0xC2B3FE2A Read register 'r12' (4 bytes) from hardware: 0x8808FE1F Read register 'sp' (4 bytes) from hardware: 0x8035FE1F Read register 'lr' (4 bytes) from hardware: 0xFFFFFFFF Read register 'pc' (4 bytes) from hardware: 0xB4050000 Read register 'xpsr' (4 bytes) from hardware: 0x00000001 Setting breakpoint @ address 0x000005B8, Kind = 2, Type = THUMB, BPHandle = 0x0001 Setting breakpoint @ address 0x000005E0, Kind = 2, Type = THUMB, BPHandle = 0x0002 Setting breakpoint @ address 0x000005E4, Kind = 2, Type = THUMB, BPHandle = 0x0003 Setting breakpoint @ address 0x0000081C, Kind = 2, Type = THUMB, BPHandle = 0x0004 Setting breakpoint @ address 0x00003864, Kind = 2, Type = THUMB, BPHandle = 0x0005 Starting target CPU... ...Breakpoint (set by 'GDB') reached @ address 0x000005B8 Reading common registers: Read register 'r0' (4 bytes) from hardware: 0x00000000 Read register 'r1' (4 bytes) from hardware: 0xC3FF0000 Read register 'r2' (4 bytes) from hardware: 0x00000000 Read register 'r3' (4 bytes) from hardware: 0x1CC10140 Read register 'r4' (4 bytes) from hardware: 0x0409FE1F Read register 'r5' (4 bytes) from hardware: 0x2409FE1F Read register 'r6' (4 bytes) from hardware: 0x2409FE1F Read register 'r7' (4 bytes) from hardware: 0x7835FE1F Read register 'r8' (4 bytes) from hardware: 0x0ADBD93C Read register 'r9' (4 bytes) from hardware: 0xD93C3897 Read register 'r10' (4 bytes) from hardware: 0x7C9F9F82 Read register 'r11' (4 bytes) from hardware: 0xC2B3FE2A Read register 'r12' (4 bytes) from hardware: 0x8808FE1F Read register 'sp' (4 bytes) from hardware: 0x7835FE1F Read register 'lr' (4 bytes) from hardware: 0xFFFFFFFF Read register 'pc' (4 bytes) from hardware: 0xB8050000 Read register 'xpsr' (4 bytes) from hardware: 0x00000001 Removing breakpoint @ address 0x000005B8, Size = 2 Removing breakpoint @ address 0x000005E0, Size = 2 Removing breakpoint @ address 0x000005E4, Size = 2 Removing breakpoint @ address 0x0000081C, Size = 2 Removing breakpoint @ address 0x00003864, Size = 2 Read 4 bytes @ address 0x000005B8 (Data = 0xF80AF000) Reading 64 bytes @ address 0x00000000 Reading 64 bytes @ address 0x00000040 Reading 64 bytes @ address 0x00000580 Reading 64 bytes @ address 0x000005C0 Reading 64 bytes @ address 0x00000600 Reading 64 bytes @ address 0x00000640
The Debugger opens up and allows me to step through code, but softwarechanges dont apply(I assume since erasing doesnt work). I also get problems with stepping through my code, I land in random spots of my application. I'm not properly going through startup-code and Jump into my main.c. Even Breakpoints do not work properly.
I already tried out swapping to another EK-RA6M1 Board and J-Link.
Anyone might have an Idea?