Unable to flash program

I just started using Renesus but I don't know what files to flash. which I followed the manual by selecting Intel .hex 

After receiving the .hex file, I opened Renesas Flash Programmer V3.15 and followed the steps, but an error occurred as shown in the picture. Where should I set it? please explain to me.

error

Renesas Flash Programmer V3.15.00 [1 Apr 2024]
Loading Project (C:\Users\Tiraporn\Documents\Renesas Flash Programmer\V3.15\Test1\Test1.rpj)
Loading File (C:\Users\Tiraporn\e2_studio\workspace\Project_LED\Debug\Project_LED.hex) CRC-32=AFEBAD66

Target device : RA

Connecting the tool
Tool : E2 emulator Lite (1LS038476B), Interface : SWD
Emulator's supply power : OFF
Emulator's firmware version:3.04.01.000
Connecting to the target device
Connecting to the target device
Communication speed : 3.0 MHz
Signature:
Device: RA
Device Code: 00390447

Erasing the selected blocks
[Code Flash 1] 0x00000000 - 0x0000FFFF size : 64 K
[Data Flash 1] 0x40100000 - 0x40100FFF size : 4 K

Writing data to the target device
[Code Flash 1] 0x00000000 - 0x00002E7F size : 11.6 K
[Config Area 1] 0x01010018 - 0x01010033 size : 28

Verifying data
[Code Flash 1] 0x00000000 - 0x00002E7F size : 11.6 K
Setting the target device

Disconnecting the tool
Error(E300010A): The data do not match. (Address: 0x00000000)
Operation failed.

Parents Reply Children
No Data