RA6M5 r_spi_write_read_common is returning FSP_ERR_IN_USE after the second frame to send

Hi,

Like i said in the title, is there something i'm missing in the pictures below?

I can't get into my callback function neither the interrupt function of the transmit interrupt. I'm using DTC because it's the only module that I can see the data output to my logic analyzer, with only the dmac I can't get it to show in my logic analyzer.

Parents Reply Children