Error 0x00030800 The reset pin of target cannot be controlled.Check the state of RESET pin.

While using E2 lite emulator ,after running the program I am getting the following error:

Error 0x00030800 The reset pin of target cannot be controlled.Check the state of RESET pin.

Following this I am getting the message shown below:

Launching Test Debug(1) has encountered a problem.
Error in final launch sequence.GDB port number not retrieved .

Please suggest some ways I can troubleshoot this condition.

Parents Reply Children
No Data