External Debugger with EK-RA8D1 (Debug In Mode)

Has anyone used an external Debugger with the EK-RA8D1?  I have tried a J-link Plus connected J13 and I have tried a J-Link LITE connected to J20.  I have jumpers J6 & J9 and all of J29 installed.  J8 is installed on pins 1&2.  I have tried with the EK powered through J10 or through J11 (Device mode). 

I get a message like this:

I am designing my own RA8D1 board, and I want to verify the pins for an external debugger.

Any insight would be appreciated!

Parents Reply
  • What is a J-Link Base?  What connector are you using for J-Link - J20 or J13?  I have connected a 5V bench power supply to TP7 and TP9 - power should not be an issue.

    When connecting power to J10, I never saw a window to select which debugger.  If J9 is installed (holding U7 in reset), how would e2 studio detect 2 debuggers?  Your response is inconsistent.  

    Dirk

Children
No Data