Hello,
So, I have been working on making a simple project to know how to configure GPIO and UART. So I did this code in a Flat Project (without RTOS). I am just starting to learn how to code so please forgive me if my code is not that well written.
void user_uart_callback(uart_callback_args_t *p_args) { (void)p_args; } void hal_entry(void) { bsp_io_level_t button_status; uint8_t buf[] = "For Testing Only.\r\n"; R_SCI_UART_Open(&g_uart6_ctrl, &g_uart6_cfg); while(1) { if(FSP_SUCCESS == R_IOPORT_PinRead(&g_ioport_ctrl, BUTTON, &button_status)) { if(button_status == BSP_IO_LEVEL_LOW) { R_IOPORT_PinWrite(&g_ioport_ctrl, LED1, BSP_IO_LEVEL_HIGH); R_SCI_UART_Write(&g_uart6_ctrl, buf, sizeof(buf)); R_BSP_SoftwareDelay(100, BSP_DELAY_UNITS_MILLISECONDS); } else { R_IOPORT_PinWrite(&g_ioport_ctrl, LED1, BSP_IO_LEVEL_LOW); } } R_BSP_SoftwareDelay(100, BSP_DELAY_UNITS_MILLISECONDS); }
So this code is working. But when I copied this to a new Flat Project (with FreeRTOS) the code failed to download and shows this error.
How to solve this?
Please take note that I didn't touch the FreeRTOS stack but it is automatically added since this is a project with RTOS. But I configured the UART the same as the first project with no RTOS.
Thank you!
Hi,Thank you for posting your question online.Can you please specify which device do you use?Best regards,Panos
EK-RA6M5
Device: R7FA6M5BH3CFC
Thank you for your response.Can you please share your project here or via private message?Thank you,Panos
Hi, I am just working on a simple UART/GPIO configuration. I just copy and pasted the same program from Flat(no RTOS) to Flat(with RTOS). Above is my working code.
I can't run the code with RTOS.
The error indicates that something is wrong with the debugger, trying to download the code to MCU.Is your build successful? Did you have any errors?Is your debugger configuration properly set? Can you share the whole console logs?Additionally, try to create a new blinky RTOS project and verify that this works.
Yes, build is successful.
I tried to make a new project with no RTOS. But I still get the download error after debug. I already did uninstall and reinstall the e2 and still I got the same error.
hi, anyone knows how to fix the debug?
Dear Jonie,Can you please check if all jumpers are set to the default configurations?Then, if the error persists, please try a new blinky project with the following configurations:Additionally, when you connect the EK board to your PC, you should see the J-link driver on the device manager
Please let us know if this suggestion was successful, otherwise we might need a full description of your actions from the start till the time you try to debug the MCU.Thank you,Panos
Hi, yes I can see the J-link driver. So, I tried it on another pc because I thought it was just my application that gave me the error or maybe i clicked something I shouldn't. I made a new project just turning on and off the user LED. I still have this message. What should I do?