Threadx Threads with thread input generated by FSP 5.20 possible?

Hello,

Is it possible with FSP Configurator to create threads with entry input?

Threadx Docs have this example:

I dont see any options in the FSP Configurtor where this might be possibile to do.

Looking at the generated code for a thread I see this:

If not possible, do i have to create threads without fsp configurator?

Best Regards

Joe

Parents Reply Children
No Data