IDAU configuration - Using MCUBOOT with a Flat project

Hello,

- We are using FSP v5.1.0 for RA, we are creating project with non-Trustzone (Flat project) using MCUBoot and an application SW.

- When looking to IDAU regions define for MCUBoot (flat project), we have the below setting:

- When looking to IDAU regions define for application SW (flat project), we have the below setting:

< Questions >

1- Having a MCUBoot and an application SW what will the IDAU regions to set-up?

2- We noticed that as we are using Non-TrustZone (Flat projects for both MCUBoot and application SW), R_BSP_SecurityInit (setting CFS1 and CFS1)) is not called.

Therefore in case of flat project what will be the incidence of setting IDAU regions ?

In advance thank you for your responses