Hi,
I have EK-RA6M4 development board and installed FSP5.5.0. When i try to debug any of example project, debugger halts at lauch because of not to find smart bundle file. When i check the debug folder that .sbd file supposed to be in it, does not include the sbd file. I deleted the debug folder , cleaned the project and built again but sbd file never had generated. How can i generate the sbd file.
Regards,
I have the same problem.
> Did you Generate Project Content, before building the project?Did you try this?
I have tried many way. Generating project content, deleting the Debug folder, and re-importing the project. None of them worked.
For my solution steps,1. Uncheck folder properties "read only" check box2. Run e2studio as admin3. Try to build see if have sbd file4. If no, delete project from list. And then import it back5. Build againAfter these work the sbd file is generated again. I dunno if this work for you but maybe worth trying.
Good luck!