I have previously used the segger emwin project with the FSP 5.4 in which my project worked fine,I have recently updated my FSP version to 5.6 after updating the FSP version i can't able to run the segger emwin project the code has been compiled and flashed into the board successfully but only the backlight of the display is on but the actual content is not displaying. i have checked this with sample segger emwin project i am faceing the same issue with the sample code too.can someone help me to solve this issue