R7FA4M2AD3CFM Pinout

Hi, 

I'm new on RA MCU, and I need to interface a Serial Flash via QSPI, currently I can't find the R7FA4M2AD3CFM pinout to come out the schematic.

Would like to ask where can find the 64pin Pinout diagram, the hardware manual didn't show which pin as a group to use for QSPI, I found :-

QSPCLK link to pin 48 and pin 49

QSSL link to pin 21 and pin 37

QIO0 link to pin 46

QIO1 link to pin 47

QIO2 link to pin 44

QIO3 link to pin 24 and pin 45

Thanks in advance

Best regards,

Neoh.K.L.

Parents Reply Children