aws_https_client_ek_ra8m1_ep Ethernet connection does not work

Hi,

I'm using EK RA8M1 to test out the aws_https_client_ek_ra8m1_ep example which fails to connect to internet, using fsp 5.7.0

Board:   EK-RA8M1
Device:   R7FA8M1AHECBD
Core:   CM85
Toolchain:   GCC ARM Embedded
Toolchain Version:   13.2.1.arm-13-7
FSP Version:   5.7.0
Project Type:   Flat

Upon compiling and running the project, the following occurs (J61 jumper is removed)

00> --------------------------------------------------------------------------------
00> Ethernet adapter Configuration for Renesas EK-RA8M1: Pre IP Init       
00> --------------------------------------------------------------------------------
00> 
...
00> Ethernet adapter for Renesas EK-RA8M1:
00>   Description                       : Renesas EK-RA8M1 Ethernet
00>   Physical Address                  : 00-11-22-33-44-54
00>   DHCP Enabled                      : No
00>   IPv4 Address                      : 0.0.0.0
00>   Subnet Mask                       : 255.255.255.0
00>   Default Gateway                   : 0.0.0.0
00>   DNS Servers                       : 0.0.0.0
00> Waiting for network link up...

But the link never comes up, no matter how long I wait. The same issue occured with fsp 5.6.0 btw.

Testing with NetX_https_client_ek_ra8m1_ep results i proper connection

00> INFO : ADC module initialization successful.
00> 
00> 
00> INFO : Checking for Ethernet link...
00> 
00> 
00> INFO : Acquired the IP address via DHCP successfully!
00> 
00> 
00> Successfully pinged DNS Server : 10.0.0.1
00> 
00> 
00> INFO : Getting IP from Adafruit Server...
00> 
00> 
00> DNS lookup is successful and the IP address of the Adafruit server is : 52.54.163.195
00> 
00> 
00> INFO : HTTPS Client is connected to the server successfully!
00> 
00> 
00> HTTP Client address is : 10.0.0.236
00> 
00> 
00> INFO : Adding an initial data on the feed...
00> 
00> 
00> INFO : Processing Post Request....
00> 
00> 
00> INFO : Posted initial data on the feed successfully!
00> 
00> 
00> HTTPS Menu Options: 
00> 1.POST Request 
00> 2.PUT Request 
00> 3.GET Request 
00> User Input: 
00> 

Similarly NetX_dhcpv4_client_ek_ra8m1_ep also operates as expected

00> INFO : Network Initialization completed successfully.
00> 
00> 
00> INFO : Checking Ethernet Link...
00> 
00> 
00> INFO : Ethernet link is up.
00> 
00> 
00> INFO : DHCP client is running.
00> 
00> 
00> INFO : DHCP client is assigned an IP address.
00> 
00> 
00> DHCP Client address is : 10.0.0.236
00> 
00> 
00> DHCP Server address is : 10.0.0.1
00> 
00> 
00> INFO : Successfully Pinged DHCP Server.
00> 
00> 
00> Lease time(in ticks) : 4320000
00> 
00> 
00> INFO : DHCP Client is reinitializing...
00> 
00> 
00> INFO : DHCP client restarted.
00> 
00> 
00> INFO : DHCP client is assigned IP address lease for second time.
00> 
00> 
00> Successfully pinged DNS Server : 10.0.0.1
00> 
00> 
00> Successfully pinged DNS gateway : 10.0.0.1
00> 
00> 
00> INFO : Released IP address back to Server.
00> 
00> 
00> INFO : DHCPV4 Client EP completed.
00> 

No modification to code was done, examples were just compiled and loaded onto the device J61 was not populated. Any idea what is wrong with aws_https_client_ek_ra8m1_ep  example and how to fix it?