Ethernet issue with the custom board

In the custom board while checking the ethernet pin we are facing the error with the ethernet all the pin of the EVK and our custom boards are same the only difference between the those two boards where the reset pin the EVK has the reset pin as 706 and our board has 404. i am trying the ethernet_ek_ra8m1 sample code it shows the network is down even after i connect the the ethernet which is working fine with the EVK,can you tell me how to configure the RESET pin in the sample code or why i am facing this issue