Hello Renesas Engineering Community Team,
I'm trying to execute a function (to stop a Timer) while breaking program execution in Debug Mode.
I'm using the on-board E2 Lite on FPB-RA2E1
But the Option to Execute Function after stopping user program is disabled (Grayed Out) in Debug Tool Settings.
Even if I change the Debugger to E2 in the Debug hardware settting, the option is not available.
Please help us solve this issue. This facility is imperative for our Application Development.
Thanks and Regards,
Vikram
Hi Vikram,
As far as I know this function is not available for the RA devices, but you can do something similar using the Breakpoint Actions menu on the Breakpoint properties.
See more about it here:Calling (Debugging with GDB)Set Breaks (Debugging with GDB)Thank you,
Andre
Dear Andre,
Thanks for your reply.
I however, don't understand how a timer can be stopped while triggering a breakpoint placed in an unrelated code area.
This is of critical importance because we are triggering thyristors with the timer outputs and hardware one-shot mode is not available in the RA2E1 and we depend upon timer interrupts to stop the timer from triggering the thyristors again.
If the timer runs uncontrollably, say when the program execution is stopped while debugging, either by a breakpoint or by a manual "Suspend" command, the power circuits will be damaged.
Please let me know if anything can be done to prevent this issue.
Regards,
Vikram.
Dear Vikram,
Thank you for your query.
To help us investigate this further, could you please provide the following details:
Which version of e² studio and FSP are you using?
Have you tried checking this option with any other RA device or a different debugger?
Could you briefly describe your project setup...for example, are you using the Timer module through FSP or configuring it manually?
These details will help us check if the behavior is specific to your setup and suggest suitable alternatives.
Kind regards,
PS
Dear PS,
We are using the E2 Studio 2024-07 and FSP version 5.4.0.
We are using the Timer Module (GPT) through FSP but can write code manually if needed.
It is clearly stated in FSP Documentation that the One-Shot mode is implemented in Software:
The GPT timer does not support one-shot mode natively. One-shot mode is achieved by stopping the timer in the interrupt service routine before the callback is called. If the interrupt is not serviced before the timer period expires again, the timer generates more than one event. The callback is only called once in this case, but multiple events may be generated if the timer is linked to the Transfer (r_dtc).
Please advise on the same,
Thanks and Warm Regards,
Thank you for your response!
The start/stop facility is not supported on devices that do not feature a Cortex-M33 or Cortex-M4 core. This is because the feature relies on a debug monitor interrupt, which is only available on these cores.
For a detailed explanation, please refer to the official Renesas document's page 43 of this document:
E2 Emulator, E2 Emulator Lite Additional Document for User's Manual (Notes on Connection of RA Devices)
specifically outlines the limitations and conditions under which the start/stop facility can be used. We recommend reviewing that section for complete clarity on this feature's applicability.
To be clear, I never tested it with RA2E1, but it works for RA6T2. Check the attached file.
Thank you
RA6T2_Breakpoint.pptx
Dear All,
Thank you very much for the Feedback.
Please let me know when you test it, if it worked on your side.
But in my experience working on motor control and digital power control, I avoid breakpoints like the plague while the power stage is on. First, there's not much you can read/evaluate from a power stage after it stops. Second, I avoid running application on the same MCU that is running the control, just essential code should run along with the control.
Your product or development maybe be completely different from what I know, so, just ignore my comment if it doesn't apply.
Thank you,