I'm using the RA8D1 for OTA. Use dual bank Mode of routines (www.renesas.cn/.../ra8-mcu-advanced-secure-bootloader-design-using-mcuboot-and-code-flash-du (albank-mode?language=en), I saw that the level of MCUboot logging can be set. I chose error and found that the project reported an error as follows. Is there a way to solve it
See how the log function is implemented.
Where can I find it?