Hello,
I've recently developed a new PCB with a RA6M5 as the MCU. And following the outline as specified in the E2Lite manual have set up a 10 pin header to interface from the RA6M5 to the E2Lite. However whenever I try to connect to the MCU in any way it always errors out. When trying to run the debug image for the MCU through e2studio the following error pops up:
When trying to access the MCU through the Renesas Flash Programmer to erase the image or connect I get the following error.
I also get this error when trying to change the debug state of the MCU through the Renesas Device Partition Manager in e2studio:
I am frankly lost on what else to try at this point. It's a brand new board with a brand new MCU. Any help or insight would be appreciated.