CAN baudrate Change in running Condition

Hii


I have a doubt i am making a can sniffing tool i need to change CAN baudrate in mid of the running condition, did there is a way to change the baudrate in mid of the ruuning condition. first when the MCU is running then the baaudrate is default like which is availble in the CAN stacks.

Thanks & Regards,

Nikhil

Parents Reply Children