RA0E1- Unable to access SWD/UART with flash programmer

 Hello,
       At first by using Renesas Flash programmer., I have performed a target read using SWD for the code flash (all blocks), data flash (1 KB), and config area (36 Bytes), all of which were in a 0xFF state. I then wrote to the code flash (all blocks), including block 0 with random data. Following this, I was unable to access the RA0E1 target via SWD, An error (E4000003) is shown during the connection attempt.
Even when tried with UART interface also displays error (E3000105)
    

 what could be the cause of this issue? or what steps can I take to recover it?
any suggestion would be greatly appreciated.
Thanks.

Parents Reply Children
No Data