Download to emulator error- Emulator firmware did not reach specified state

Hi Renesas community .

I was trying to download  a program to my RA6M1 suddenly this error message is coming .What could be the issue please help by giving suggestions to resolve.

Parents
  • Hi,

    The error 0x00070100 indicates a timeout due to the emulator not reaching the expected target state.

    Please check the following:

    1. If your design includes multiple reset sources (e.g., external supervisor, manual reset, etc.), ensure they are not interfering with the emulator’s control of the MCU reset line.
    As a test, try directly connecting the emulator’s reset pin to the MCU’s reset pin to bypass any intermediate logic and confirm stable behavior.

    2. Confirm the target board is powered, and all key signals (RESET, TOOL0/FINE, GND) are properly connected.

    3. Verify correct MCU part number, interface (FINE/JTAG), and clock settings in e² studio.

    Let us know if the issue persists or if you’d like us to review your setup.

    Kind regards,
    PS

Reply
  • Hi,

    The error 0x00070100 indicates a timeout due to the emulator not reaching the expected target state.

    Please check the following:

    1. If your design includes multiple reset sources (e.g., external supervisor, manual reset, etc.), ensure they are not interfering with the emulator’s control of the MCU reset line.
    As a test, try directly connecting the emulator’s reset pin to the MCU’s reset pin to bypass any intermediate logic and confirm stable behavior.

    2. Confirm the target board is powered, and all key signals (RESET, TOOL0/FINE, GND) are properly connected.

    3. Verify correct MCU part number, interface (FINE/JTAG), and clock settings in e² studio.

    Let us know if the issue persists or if you’d like us to review your setup.

    Kind regards,
    PS

Children
No Data