Hi There, Can I use the following RTOS porting for R7F702301B( RH850U2A8 family)? Is the ISRwrapper function compatible with R7F702301B or should I make some changes?github.com/.../master
Hello,
You can find the last porting for FreeRTOS porting for RH850, including U2A8 as the below,1. With CCRH compiler:FreeRTOS-Kernel-Partner-Supported-Ports/CCRH/U2x at main · FreeRTOS/FreeRTOS-Kernel-Partner-Supported-PortsDemo: FreeRTOS-Partner-Supported-Demos/RH850_U2Ax_CCRH at main · FreeRTOS/FreeRTOS-Partner-Supported-Demos2. With GHS compiler:FreeRTOS-Kernel-Partner-Supported-Ports/GHS/U2x at main · FreeRTOS/FreeRTOS-Kernel-Partner-Supported-PortsDemo: FreeRTOS-Partner-Supported-Demos/RH850_U2Ax_GHS at main · FreeRTOS/FreeRTOS-Partner-Supported-Demos
However these are not official ports from Renesas and thus cannot be further supported.