Request for Sample Code and Project for LIN Master/Slave on RH850/F1KM-S1 (RLIN3 Interface)

Dear Renesas Support Team,

I am currently working on the RH850/F1KM-S1 microcontroller, and I am specifically utilizing the LIN/UART interface (RLIN3) for my project requirements. I would appreciate it if you could provide any sample code or reference projects demonstrating the implementation of both LIN Master and LIN Slave functionalities using the RLIN3 module.

Additionally, I would like guidance on dynamically changing the LIN baud rate during runtime, if such functionality is supported.

Your support in this regard will be highly valuable to expedite the development and validation process.

Looking forward to your response.

Best regards,
rao

Parents Reply Children
No Data