Hi,
i would like to make initial code about CLMA3's clock monitor in RH850/F1KM-S1_R7F7016894AFP.
Plz let me know the code as below.
How to enable/disable the CLMA3 .
Using dr7f7016894.dvf.h (GHS Header definition file)
like this. (E.g. Clock. / Write Protected Reg Case)
Plz share the guide code for me.
Best Regards,
David.
I want to handle this part. (5.2.3 Detail of Clock Monitor Control and Test Protection Cluster Registers / 5.2.3.1 ~ 5.2.3.4)
Plz support me.
Hello,
Clock monitoring is started by the clock monitor when CLMAnCTL0.CLMAnCLME = 1.
The correct write sequence using the CLMAnPCMD register is required in order to update this register.
The writing procedure to write-protected registers is described on chapter 5.1.2:
Thanks~
I already know your guide.
We need CLMA3 GHS/CS+ Based TEST Program as below.
Dear Renesas Expert,
Hello.
Our Customer're trying to implement a specific sequence application utilizing CLMA3 function using RH850F1KM S1 MCU.
The intention of the scenario is to use CLMA3 in the application area and deactivate it in the bootloader area.
At first,First of all, in order to use the CLMA3 register, it is judged that the Write Protected sequence must be used to change the register value.If you could share an example of how to use CLMA3 TEST that includes the code including the Initial Sequence, I think they can use it as a driver for implementing the application.
Please support them.
In addition,I have checked with TISS.
https://www.renesas.com/en/search?keywords=TN-RH8-B131A%2FE
It seems that there were some issues.
Apart from the above request, has this TISS issue been resolved?
Anyway, looking at the document content in TISS, I can guess that there is an example of a CLMA3 test conducted with the relevant content.
I would appreciate it if you could request the relevant TEST CODE.
Thanks~,
B.R
The official recommendation for the CLMA test (and all FuSa related tests) is provided in the Safety Application Note (SAN) which requires NDA to be in place. You can submit a private ticket to initiate that process.
The only way to address the issue cited by the technical update via software would be to widen the tolerance on the CLMA configuration. The TU does not mention how far out of spec the osc operates due to the defect, as such no guess can be made as to how much to widen the test.
The workarounds cite hardware methods to address the issue. Also mentioned id that if these hardware modifications cannot be implemented to contact Renesas, this would involve another private support ticket.
Hi.
Thanks your advice.
Just.. (without NDA)
First of all, in order to use the CLMA3 register, it is judged that the Write Protected sequence must be used to change the register value.If you could share an example of how to set CLMA3 Enable/Disable that includes the code including the Initial Sequence Func only,
If we can just provide this initial Func (Write Protected Enable/Disable. Each Func)
They can use it as a driver for implementing the application.
Plz support us. David.