Unable to fetch the "R_FCL_Fct_Handler" during initialization.

Hello Team,

      during initialization phase I am trying to access the function " R_FCL_Fct_Handler", got runtime error. 

      from the  function " R_FCL_CopySections" inside i am fetching the below function base address  R_FCL_Fct_Handler from RAM, since before handler function was copied into ROM to RAM area.

                 g_fcl_data_str.handlerPtr_p = (r_fcl_fctPtr_t)R_FCL_CalcFctAddr ((uint32_t)(&R_FCL_Fct_Handler)); 

after i got the handler function address, i called from that function pointer in below function, then i got crash, i am suspecting that function address not identified.  

Hints i have configured like My address in linker file:

from map file FCL_RESERVED address generated in .map file  from below 

\

and below assigned in RAM address in my code based on above .map  

above RAM address one used under the destAddr = g_fcl_data_str.RTCfg_pstr->addrRam_u32: for find the Handler function address from the RAM.

Please hlep me how to resolve this error?

Parents Reply Children
No Data