Hi,
I am using RL78/G13 with e2 studio IDE. I having a problem of Section address overflow out of range : ".SLIB"
My code size was shown as larger than my controller size. But I didn't increase any script in a project even my backup project also I can't Build, That same error came.
So I doubted in IDE. I was tried many things but I can't to solve this issue.
Is anything I want to change or check. I was attached details in below .Please check and give a solution for this.
Renesas Optimizing Linker (W3.06.00 ) 27-Feb-2024 11:40:12 *** Options *** -subcommand=LinkerFCM360W_TEST_050224.tmp -MAKEUD=J:\UKM\renesas\my_renesas_project\e2_studio\workspace\FCM360W_TEST_050224\HardwareDebug/FCM360W_TEST_050224_l.ud -device="C:/Users/ukm/.eclipse/com.renesas.platform_1435879475/DebugComp/RL78/RL78/Common/DR5F100LG.DVF" -list="FCM360W_TEST_050224.map" -nooptimize -entry=_start -auto_section_layout -security_id=00000000000000000000 -debug_monitor=1FE00-1FFFF -user_opt_byte=FFFFEF -ocdbg=04 -input=".\generate\cstart.obj" -input=".\generate\stkinit.obj" -input=".\src\EEPROM.obj" -input=".\src\LCD_Factory_Profile.obj" -input=".\src\LCD_user_profile.obj" -input=".\src\build_props.obj" -input=".\src\firmware_NGC_3PH_backup_090124.obj" -input=".\src\https.obj" -input=".\src\https_wifi.obj" -input=".\src\lcd.obj" -input=".\src\modem_ack.obj" -input=".\src\mqtt.obj" -input=".\src\r_cg_adc.obj" -input=".\src\r_cg_adc_user.obj" -input=".\src\r_cg_cgc.obj" -input=".\src\r_cg_cgc_user.obj" -input=".\src\r_cg_intc.obj" -input=".\src\r_cg_intc_user.obj" -input=".\src\r_cg_it.obj" -input=".\src\r_cg_it_user.obj" -input=".\src\r_cg_lvd.obj" -input=".\src\r_cg_lvd_user.obj" -input=".\src\r_cg_port.obj" -input=".\src\r_cg_port_user.obj" -input=".\src\r_cg_serial.obj" -input=".\src\r_cg_serial_user.obj" -input=".\src\r_cg_timer.obj" -input=".\src\r_cg_timer_user.obj" -input=".\src\r_main.obj" -input=".\src\r_systeminit.obj" -library="C:\Program Files (x86)\Renesas\RL78\1_13_0\lib\rl78cm4s.lib" -library="C:\Program Files (x86)\Renesas\RL78\1_13_0\lib\rl78cm4r.lib" -library="C:\Program Files (x86)\Renesas\RL78\1_13_0\lib\malloc_n.lib" -output="FCM360W_TEST_050224.abs" -debug -nocompress -memory=high -rom=.data=.dataR,.sdata=.sdataR -nomessage -nologo *** Error information *** W0561120:Section address is not assigned to ".SLIB" F0563100:Section address overflow out of range : ".SLIB" *** Mapping List *** SECTION START END SIZE ALIGN .vect 00000000 0000007f 80 0 .constfAPP_VERSION_f 00000080 00000083 4 2 .constfAPI_KEYS_f 00000084 000000b3 30 2 .sdata 00000080 00000080 0 2 .option_byte 000000c0 000000c3 4 1 .security_id 000000c4 000000cd a 1 .monitor1 000000ce 000000d7 a 1 .constf 000000d8 0000014f 78 2 .constfURLS_f 00000150 000001cc 7d 2 .data 000001ce 00001525 1358 2 .text 00001526 00001cd0 7ab 1 .RLIB 00001cd1 00002a37 d67 1 .const 00003000 00009753 6754 2 .textf 00009754 0001fcb5 16562 1 .monitor2 0001fe00 0001ffff 200 1 .bss 000fcf00 000fdfdd 10de 2 .dataR 000fdfde 000ff335 1358 2 .sbss 000ffe20 000ffe20 0 2 .sdataR 000ffe20 000ffe20 0 2 .SLIB 000ffe20 00102192 2373 1
Thanks,
Hello,
The .SLIB section is too big and overflows beyond the end of memory range which is 0xFFFFF.
The SLIB section is section for code of standard libraries.
Have you included such a library in the project ?
Regards
Hi AZ [Renesas],
Thanks for your reply,
I am not include any many libraries.
I was included string library only ,I additionally used. And I generate a project with code generator So many interrupts and
communication related header files created automatically.
And I include user defined header files in my project.
The .SLIB section is by default placed in code flash.
Looking at your map file I guess that you have moved it to RAM ?
The .SLIB seems to be 2373 bytes so it cannot fit after .dataR section.
I recommend that you place .SLIB in code flash.
Hi AZ [Renesas]
No, I am not config .SLIB data store in to a RAM. When I choose to select section layout as automatically , I seen Section overflow error like above (Section address overflow out of range : ".SLIB").
If I reapply that section as like you are send section view means I had a Error like below, and I attached images below.
E0562321:Section ".monitor2" overlaps section ".textf"
Renesas Optimizing Linker (W3.06.00 ) 28-Feb-2024 08:28:46 *** Options *** -subcommand=LinkerFCM360W_TEST_050224.tmp -MAKEUD=J:\UKM\renesas\my_renesas_project\e2_studio\workspace\FCM360W_TEST_050224\HardwareDebug/FCM360W_TEST_050224_l.ud -device="C:/Users/ukm/.eclipse/com.renesas.platform_1435879475/DebugComp/RL78/RL78/Common/DR5F100LG.DVF" -list="FCM360W_TEST_050224.map" -nooptimize -entry=_start -auto_section_layout -security_id=00000000000000000000 -debug_monitor=1FE00-1FFFF -user_opt_byte=FFFFEF -ocdbg=04 -input=".\generate\cstart.obj" -input=".\generate\stkinit.obj" -input=".\src\EEPROM.obj" -input=".\src\LCD_Factory_Profile.obj" -input=".\src\LCD_user_profile.obj" -input=".\src\build_props.obj" -input=".\src\https.obj" -input=".\src\https_wifi.obj" -input=".\src\lcd.obj" -input=".\src\modem_ack.obj" -input=".\src\mqtt.obj" -input=".\src\r_cg_adc.obj" -input=".\src\r_cg_adc_user.obj" -input=".\src\r_cg_cgc.obj" -input=".\src\r_cg_cgc_user.obj" -input=".\src\r_cg_intc.obj" -input=".\src\r_cg_intc_user.obj" -input=".\src\r_cg_it.obj" -input=".\src\r_cg_it_user.obj" -input=".\src\r_cg_lvd.obj" -input=".\src\r_cg_lvd_user.obj" -input=".\src\r_cg_port.obj" -input=".\src\r_cg_port_user.obj" -input=".\src\r_cg_serial.obj" -input=".\src\r_cg_serial_user.obj" -input=".\src\r_cg_timer.obj" -input=".\src\r_cg_timer_user.obj" -input=".\src\r_main.obj" -input=".\src\r_systeminit.obj" -library="C:\Program Files (x86)\Renesas\RL78\1_13_0\lib\rl78cm4s.lib" -library="C:\Program Files (x86)\Renesas\RL78\1_13_0\lib\rl78cm4r.lib" -library="C:\Program Files (x86)\Renesas\RL78\1_13_0\lib\malloc_n.lib" -start=.const,.text,.RLIB,.SLIB,.textf,.constf,.data,.sdata/03000,.dataR,.bss/0FCF00,.sdataR,.sbss/0FFE20 -output="FCM360W_TEST_050224.abs" -debug -nocompress -memory=high -rom=.data=.dataR,.sdata=.sdataR -nomessage -nologo *** Error information *** E0562321:Section ".monitor2" overlaps section ".textf" *** Mapping List *** SECTION START END SIZE ALIGN .vect 00000000 0000007f 80 0 .constfAPP_VERSION_f 00000080 00000083 4 2 .constfAPI_KEYS_f 00000084 000000b3 30 2 .option_byte 000000c0 000000c3 4 1 .security_id 000000c4 000000cd a 1 .monitor1 000000ce 000000d7 a 1 .constfURLS_f 000000d8 00000154 7d 2 .const 00003000 00009753 6754 2 .text 00009754 00009efe 7ab 1 .RLIB 00009eff 0000ac65 d67 1 .SLIB 0000ac66 0000cfd8 2373 1 .textf 0000cfd9 0002353a 16562 1 .constf 0002353c 000235b3 78 2 .data 000235b4 0002490b 1358 2 .sdata 0002490c 0002490c 0 2 .monitor2 0001fe00 0001ffff 200 1 .dataR 000fcf00 000fe257 1358 2 .bss 000fe258 000ff335 10de 2 .sdataR 000ffe20 000ffe20 0 2 .sbss 000ffe20 000ffe20 0 2
Please check,
The debug monitor area is overlapped because the sections in code flash are now too big.
Change the address below from 0x3000 to 0x2000 so they start lower in code flash.
Also reserve the debug monitor area with this option:
No, I was changed as you are suggested , But still have Error.
Is really that memory size was overload ah, I can't to feel accept because when I rebuild my backup project are also showing this overflow error that why I can't to accept memory was full.
I know my backup projects are having 95% memory full at last build. But now I rebuild that file I got error, even I didn't include any script in same project.
Is there any idea about that ?
Not sure the address is changed because I sill see sections starting at 0x3000 and not at 0x2000.
Yes it was not changed Once I clean and rebuild that project ,after that address changed but not ERROR.
In previous screenshot the .textf was 75KB and now 91KB, how is it possible ?
The program is simply too big. The 128KB code flash ends at 0x1FFF you cannot have a code flash section that goes beyond this address.
But this was my backup project. And how now its showing section overflow and memory was too big ?
Is anything I need to check and verify for this,
I do not know the difference between this project and backup project but for R5F100xG the sections placed in code flash must not exceed 0x1FFF.
You mean not exceed 0x1FFFF ,right.
Okay we are process to arrange extend our program memory by choosing another controller in RL78.
And if I have to build in this same project in another CPU or laptop, I will update you.
Thanks for your valuable support AZ [Renesas].
Yes, I mean 0x1FFFF, my mistake.
Understood, please let me know for further issues.