What is the RL78/G14 SFR @ FFFF8H ?

Does anyone know what the undocumented RL78 SFR located at 0xffff8 is and/or what it does ?

The CRT longjmp() function appears to store the address of the jmp_buf argument into this address at the start of the function execution.

Regards,

Steven J. Ackerman

ACS, Sarasota, Florida

  • Which compiler are you using?

    Can you provide a screen-shot of what you are observing?

    I don't see this behavior using CC-RL, which is where I would expect to find any "hidden" SFR usage if there was any.  As this is a lib-function, it is not specific to G14 so this would seem very unlikely behavior.

  • Thanks for your reply.

    Using CC-RL v1.10.  Experimenting with some 'coroutines' done using setjmp/longjmp. The code basically works, but I was interested in seeing what the overhead was, so I examined the code for the two functions:

              setjmp:

    000051df:   movw    de, ax          ; point to jmp_buf arg

    000051e0:   movw    ax, sp          ; save sp into jmp_buf[0]

    000051e2:   movw    [de], ax

    000051e3:   movw    ax, [sp]        ; save return address into jmp_buf[1]

    000051e5:   movw    [de+2], ax

    000051e7:   movw    ax, [sp+2]

    000051e9:   movw    [de+4], ax

    000051eb:   clrw    ax              ; return zero

    000051ec:   ret    

                       longjmp:

    00005146:   movw    de, ax                        ; special treatment of jmp_buf[0] arg…

    00005147:   movw    ax, [de]

    00005148:   movw    0xffff8, ax                 ; is this accessing the sp ?

    0000514a:   movw    ax, [de+2]                 ; restore return address from jmp_buf[1]

    0000514c:   movw    [sp], ax

    0000514e:   movw    ax, [de+4]

    00005150:   movw    [sp+2], ax

    00005152:   movw    ax, bc                        ; check val == 0, and return 1 instead

    00005153:   cmpw    ax, #0

    00005156:   sknz   

    00005158:   incw    ax

    00005159:   ret    

     

    Steven J. Ackerman

    ACS, Sarasota, Florida

  • Hello,

    Yes, this is the address stack pointer register:

    https://www.renesas.com/us/en/document/mah/rl78-family-users-manual-software-rev230

    Also, I would recommend updating to the latest CC-RL 1.13.

  • Thank you.

    I had this manual, but didn't look in it for this SFR. This table of fixed SFRs doesn't appear in the G13 or G14 hardware manuals.

    I wonder why this addressing mode was used instead of MOVW SP, AX...

    Oh well, thanks for clearing that up.

    Steven J. Ackerman

    ACS, Sarasota, Florida

  • I believe what you are seeing is a result of the disassembler rather than using a different insn.

    00005148:   movw    0xffff8, ax                 ; is this accessing the sp ?
    0000514a:   movw    ax, [de+2]                 ; restore return address from jmp_buf[1]

    It would appear that the insn "movw 0xFFF8,ax" is only 2-bytes (0x514a - 0x5148), which tells me that the disassembler has interpreted the "movw sp,ax" as what was displayed.  If you can view the opcode / operand this could be confirmed.  Opcode "BE" is the 2-byte insn for "movw sfr,AX" while the "BF" opcode would be the 3-byte insn "movw !addr16,ax".