How to separate flash memory

Hi team,

            The controller RL78_G23-(R7F100GSN2DFB) have 768 KB code flash memory. controller should need to keep the main application code & RL78_G13 application code. So that purpose the flash memory was needed to separate two sections. So how to make this appropriate setting in RL78_G23 controller. please let me know

Parents Reply
  • 1.It may be possible to send .MOT file from RL78_G23 µC to RL78_13 µC without RFD file?

    2.How to separate the memory section. below given image taken from Renesas sample software.

    in this image where should i start separate the memory section.

    3.But in the Reference Manuel the code flash memory was commonly given. shown in below attached

    image  

      

    Kindly clarify the where should i start to separate the memory section

Children