Hello,
I don't see the option to enbale the SNOOZE mode for the chip in CS+.
And any sample code would be appreciated.
Thanks
...
The CS+ Code Generator does not support SNOOZE mode of Serial Array Unit. This means that you will need to add your own code to enable and use this function. Note that only CSI00 can be set to the SNOOZE mode.
Please go through section 14.5.7 which describes in detail the settings for Snooze mode:
https://www.renesas.com/en/document/mat/rl78l13-users-manual-hardware?r=479566
It is crucial that the SWCm bit of serial standby control register m (SSCm) to 1 just before switching to the STOP mode.
Hi,I found this AN R01AN0957EJ0100 but not able to find the sample code.
Can you please share it.
Thank you in advance!
Here is the associated sample code:
www.renesas.com/.../rl78g13-low-power-consumption-operation-csi-snooze-mode-cc-rl-rev100-sample-code