External Interrupt not triggered in RL78/G22 mcu

Hi team,

I am using the RL78/G22 mcu with Fast prototyping board to develop the PWM output. In my scenario, I am using the switch as an external interrupt to trigger. But the interrupt function is not triggered when the switch was pressed, also the output duty cycle is 100% when I do a build and run the code. what is the issue here?