Inquiry Regarding Power Modes for R5F10RGCGFB in a Digital Timer Application

Dear Renesas Support Team,

We are currently using the R5F10RGCGFB microcontroller in our digital timer application. While reviewing the datasheet, we came across the following power-saving modes:

  • Ultra-low power consumption technology
    • VDD = single power supply voltage of 1.6 to 5.5 V
    • HALT mode
    • STOP mode
    • SNOOZE mode

Our concern is as follows:

If the power supply to the digital timer is cut off, we need to ensure that the current time and user-inputted data are retained while consuming the least amount of battery power. Among the available power-saving modes, which one would be the most suitable for achieving this requirement?

We would appreciate your guidance on the best approach for our application.

Best regards,

LEE

Parents Reply Children
No Data